2014-07-04 5:17 AM
I have to get started for STM8S003F3. I have made a custom board.
1. What debugger to choose?2. What IDE, freeware preferably for c language3. Any example code to get started2014-07-04 6:07 AM
If you are writing small applications then IAR have a free development environment (IDE/Compiler/Debugger) for non-commercial use.
If you don't want to go down the standard library route then about using the registers to control the STM8S.Regards,Mark2014-07-05 8:32 AM
STM8S003F3P6 STM8 Minimum System Development Board SWIM Debug
http://www.icstation.com/product_image.php?products_id=2745
I initially used the IAR C compiler for the STM8 and ended up buying some fo the cheap STLINKV2 clones, again from eBay. They work with the IAR product under Windows, and more importantly for me, they work with the stm8flash command line utility for Linux. As I am a hobbyist, the IAR product was pretty overwhelming (let me restate: I'm a Very Casual Hobbyist) and also wanted a Linux development environment. The SDCC compiler now supports (limited) STM8 application building, certainly more than adequate for my humble needs. The SourceForge site has the relevant STM8 stuff for SDCC as well as some examples. I noted that the 'simple blinky LED' example relies on the ADC and interrupts, a tad exotic for my tastes. http://sourceforge.net/directory/os:linux/freshness:recently-updated/?q=stm8 -there is an SDCC port for Windows as well I believe. Finally I found that the site by Mark Stevens called 'Silverlight Developer' http://blog.mark-stevens.co.uk/the-way-of-the-register/ is a fabulous site, helped me to (somewhat) understand the low-level register setups of the STM8 products. I see that he's responded to your post and I can vouch that its a great site. If you're running under linux, I don't think you can use the debugging features of SWIM. Hope this helps Good Luck Terry2014-07-21 11:42 PM
Hi,
I recommend COSMIC compiler as on F003 programs always need to be optimized - I tried IAR and Raisonance and both where buggy especially on highest optimization levels. Advice from Raisonance was to not use optimization... ;-). So far Cosmic performed best. As Debugger I use RLINK but I think there are cheaper ones that can do the same. Best regards, Alex2014-08-01 8:12 AM
1. As hardware debugger use Discovery board. It's cheap, and you can use its own MCU as target.
Or use Chinese clone of ST-LINK - lots of them on ebay.
2. As IDE and software debugger I reccomend to use IAR EWB. It's free with code size limitation of 8 kbytes - it's more than enough for start. 3. Examples of code - look here: