2016-09-28 06:36 AM
I've downloaded STVD, installed it, Downloaded Cosmic C, installed it and downloaded en.stsw-stm8069.zip (standard peripheral library) Now. I cannot for the life of me get this thing working. I opened the .stw project within the unzipped std perph lib and when I build the stm8s105 project I get ''The Executable Cannot be found'' you can fix it by edit......
I try and fix it but I have no idea what it wants me to do.Thanks Bill #stm8s-discovery2016-09-29 02:26 AM
Hi Bill,
When a project is added to the workspace it will ask which toolchain one is using. Alternatively you can set it in Project->Settings (General tab). Obviously the root path needs to be set to where ever you installed the toolchain. Hope that helps. Thanks, Ian