2018-01-29 8:02 AM
When I try to compile my project or the standard project, I get the message -clDebug \ -coDebug \ main.c #error cpstm8 C: \ Program Files (x86) \ COSMIC \ CXSTM8_32K \ Hstm8 \ mods0.h: 1 FlexLM No such feature exists.I copied the license file to the correct folder, Cosmic CxSTM8 32K and STToolset were installed on the PC. The error is present on two different systems XP and Win7. Reinstalling software does not solve the problem. How can I fix this problem?
2018-01-29 9:53 AM
Hello,
the 32k version you are trying to use is old and not supported anymore: get the new version without any limit
http://cosmicsoftware.com/download_stm8_free.php
and the problem will go away.Regards,
Luca