2009-11-13 10:22 PM
Flash Loader Demonstrator V2.1.0 Release
2011-05-17 6:05 AM
Dear Community,
We are releasing a new STM32â„¢ and STM8â„¢ Flash loader demonstrator that Contains the Demo GUI, Command line and header source files using UART protocol : Version 2.1.0http://www.st.com/stonline/products/support/micro/files/um0462.zip
V2.1.0 - 11/02/2009 ===================== New Features ************ + Adding New STM8 map files with options bytes support, + Adding ''Echo'' mode option in UART communication for LIN emulation over UART for STM8 + Adding a new combox with ''No erase'' option when downloading a file. Enhancements ************ + Fix of COM ports number > 9 using when using some USB-to-Serial commercial bridges, + Fix of --o option (removes FFs data) when using Command line utility, + Fix of GUI map files selection in some particular cases, + Fix of refresh of the window values after reading Options Bytes, + Removing ''Stop Bits'' combox in the GUI first Window, + Removing CAN selection over the COMBox bridge board, + Removing DFU Selection for the GUI; To use DFU bootloader refer to DFuSe Software, + Minor enhancements for dialog box messages and comments for the GUI and Command Line versions. Known Limitations ***************** + Automatic selection of some STM8 devices may not work properly. If required, use command line version with batch files customization. Cheers, STOne-32