cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST-Link/V2 support STM8S103F3 ?

AkhilKumar
Associate II

Dear All,

I started working on the STM8S Mcu's recently. Here I have some basic queries.

1)By using this ST-Link V2 in circuit debugger and programmer. (ST-LINK/V2 - ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32 - STMicroelectronics) Can we use it for both flashing and debugging to this STM8S103F3 Mcu?

2)Can I use STVD application alone for both flashing and debugging to my Mcu? or

3)STVP application is also required? (but STVP is flash programmer right)

Please any one can guide me to get clear understandings of this queries.

Thank you in advance!

Best regards,
Akhil Kumar.

1 ACCEPTED SOLUTION

Accepted Solutions
gabs
Associate II

1) Yes, this is the tool for debugging and flashing.

2) STVD will flash and debug, for flashing only it doesn't look practical, go for STVP.

3) Yes if you plan to go into production, STVP also offer a command line option.

 

Regards.

View solution in original post

5 REPLIES 5
gabs
Associate II

1) Yes, this is the tool for debugging and flashing.

2) STVD will flash and debug, for flashing only it doesn't look practical, go for STVP.

3) Yes if you plan to go into production, STVP also offer a command line option.

 

Regards.

AkhilKumar
Associate II

Hello Gabs,

Thank you so much for your quick response.

Above 2 and 3 points: I have concluded like this We can flash the program to mcu using STVP and we can start the debugging using STVD in that case, right? 

Please Correct me if am wrong.

 

Best regards,

Akhil Kumar.



 

gabs
Associate II

If you are only developing/debugging the code, you don't need STVP, STVD will flash de code before the debug session starts. 

You need STVP when you start production, STVP is for memory flashing only.

 

Regards

AkhilKumar
Associate II

Thank you gabs for your quick response and support.

mschn.17
Associate II

The open source project stm8flash will also flash this part using stlink v2 and clones. Best part is, that you can specify the stlink serial number on the command line in case you have more than one connected at one time. f.i if you need to flash one stm32 and another stm8 with the same production rig. stm8flash has almost 0 dependencies and will compile and run effortlessly for both windows and linux.