DAC Module with Timer 4 trigger
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-15 5:04 AM
Hello,
I am working on STM8L-Discovery DAC module.
I have used Timer 4 trigger (1Khz) and DMA transfer is enabled.
But my DAC_OUT1 pin PF0 isn't giving a sine wave.
I want to know what mistake I might have done.
Thanks in advance.
Regards,
Sandeep
Tool Used - IAR Workbench
Code-
#include "stm8l152C6.h"
uint16_t Sinus12bit[130] = {1800, 1887, 1974, 2060, 2146, 2231, 2315, 2397, 2479,
2559, 2637, 2713, 2786, 2858, 2927, 2994, 3057, 3118,
3176, 3230, 3281, 3329, 3373, 3414, 3450, 3483, 3512,
3537, 3558, 3574, 3587, 3595, 3599, 3599, 3595, 3587,
3574, 3558, 3537, 3512, 3483, 3450, 3414, 3373, 3329,
3281, 3230, 3176, 3118, 3057, 2994, 2927, 2858, 2786,
2713, 2637, 2559, 2479, 2397, 2315, 2231, 2146, 2060,
1974, 1887, 1800, 1713, 1626, 1540, 1454, 1369, 1285,
1203, 1121, 1041, 963, 887, 814, 742, 673, 606, 543, 482,
424, 370, 319, 271, 227, 186, 150, 117, 88, 63, 42, 26, 13,
5, 1, 1, 5, 13, 26, 42, 63, 88, 117, 150, 186, 227, 271, 319,
370, 424, 482, 543, 606, 673, 742, 814, 887, 963, 1041,
1121, 1203, 1285, 1369, 1454, 1540, 1626, 1713};
void SetPowerRegisters(void)
{
PWR->CSR1=0X0B; // PVD on, Threshold 2.85 V
RST->SR=0xff;
}
void SetClock(void)
{
CLK->CKDIVR = 0x00; // No Clock Division
CLK->CRTCR = 0x00; // No RTC clock selected
CLK->ICKCR = 0x01; // HSI On
CLK->PCKENR1 |= 0x84; // DAC and TIM4 clock enabled
CLK->PCKENR2 |= 0x20; // DMA1 clock enabled
//CLK->PCKENR3 |= 0x08;
CLK->SWR = 0x01; // HSI as system clock
}
void SetPort(void)
{
GPIOE->DDR |= 0x80;
GPIOE->CR1 |= 0x80;
GPIOE->CR2 |= 0x80;
GPIOE->ODR = 0x80; // LED at PE7
}
void SetTIM4(void)
{
TIM4->IER|=0x01; // Trigger and Update interrupt enabled
TIM4->CR1 |= 0x81; // Counter enable
TIM4->CR2 |= 0x20; // TIM4 TRGO selection
TIM4->SMCR|=0x00;
TIM4->PSCR |= 0x06;//0x05; // Set the Prescaler value
TIM4->DER|=0x01; // DMA Request Enable
TIM4->EGR|=0x00;
TIM4->CNTR |=0x00;
TIM4->ARR = 89;
}
void SetDAC(void)
{
DAC->CH1CR1 |= 0x05;//0x04;//0x05; // Timer 4 Trigger and DAC Channel enabled
DAC->CH1CR2 |= 0x10;//0x10;//0x30; // DMA enabled
//DAC->SR |= 0x01; // DAC underrun detection
//DAC->SWTRIGR |=0x01; // Enable Software Trigger
}
void SetDMA(void)
{
DMA1_Channel3->CCR |= 0x38; // channel 3 enabled, Memory to Peripheral, Memory Increment, Circular
DMA1->GCSR = 0xFD; // Max time out, DMA global channel
uint16_t Add;
DMA1_Channel3->CPARH = 0x53; // peripheral address
DMA1_Channel3->CPARL = 0x88;
Add = (uint16_t)&Sinus12bit[0];
DMA1_Channel3->CM0ARL = Add; // memory address
DMA1_Channel3->CM0ARH = Add>>8;
DMA1_Channel3->CNBTR = 2; // 100 no of data transfer
DMA1_Channel3->CSPR = 0x38;
}
void main( void )
{
SetClock();
SetPort();
GPIOF->DDR|=0x01;
GPIOF->ODR|= 0x00;
SetDMA();
SetDAC();
SetTIM4();
while(1)
{
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-02-15 8:54 AM
To find out the bug location, try to use the TIMER real pin and maually connect to the DAC trigger pin.
This way, you will be able to manually narrow down where is the issue.