cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM8S105 with C1 and C2 pull up no it config and TIM1 for encoder mode. TIM1 counter counts from 0 to 1 and back to 0. can anyone please help. Thanks

jf
Associate

Timer 1 inittalization code is below:

TIM1_TimeBaseInit(10, TIM1_COUNTERMODE_CENTERALIGNED1, 1000, 1);

TIM1_ICInit(TIM1_CHANNEL_1,TIM1_ICPOLARITY_FALLING ,TIM1_ICSELECTION_DIRECTTI ,TIM1_ICPSC_DIV1,0);

TIM1_ICInit(TIM1_CHANNEL_2,TIM1_ICPOLARITY_FALLING ,TIM1_ICSELECTION_DIRECTTI ,TIM1_ICPSC_DIV1,0);

TIM1_EncoderInterfaceConfig(TIM1_ENCODERMODE_TI12,TIM1_ICPOLARITY_FALLING ,TIM1_ICPOLARITY_FALLING );

TIM1_Cmd(ENABLE);

I have the following in an infinite loop after the code above runs:

TIM1_GetCounter();

When i turn my encoder whether clockwise or anti clockwise TIM1_GetCounter() returns me one and goes back to zero.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0