cancel
Showing results for 
Search instead for 
Did you mean: 

Compiling problem with Cosmic CxSTM8 16K and LONG data

mjobard2
Associate
Posted on December 21, 2010 at 16:05

Compiling problem with Cosmic CxSTM8 16K and LONG data

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Andrew Neil
Super User
Posted on May 17, 2011 at 15:11

The compiler is behaving perfectly correctly!

ISO/IEC 9899:1990 - the so-called ''ANSI C'' specification - states:

''The type of an integer constant is the first of the corresponding list in which its value can be represented. Unsuffixed decimal: int, long int, unsigned long int...''

 

If you want to force the type of the constant to be unsigned, then you need to add the suffix 'u' or 'U'...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
mjobard2
Associate
Posted on May 17, 2011 at 15:11

Works fine now... thanks for the reminder (but where is my Bible-C?!).

'Thought that the compiler would warn that signed data was compared with unsigned variables, but I guess you can not expect too much from a free compiler.

luca239955_stm1_st
Senior II
Posted on May 17, 2011 at 15:11

>> 'Thought that the compiler would warn that signed data was compared with unsigned variables, but I guess you can not expect too much from a free compiler.

can you provide an example of a compiler raising a warning for this?

Regards,

Luca

Andrew Neil
Super User
Posted on May 17, 2011 at 15:11

''Thought that the compiler would warn that signed data was compared with unsigned variables''

Other than special cases, what's to warn about?

What warning would you suggest?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.