2011-03-18 8:24 AM
I have just purchased the STM8L-DISCOVERY, I have problems getting the device communication functioning on my primary PC. I have installed all the same apps... on a secondary PC, on this PC all is OK.
On my primary PC I get:
** Connection error (usb://usb): swim error [30004]: comm timeout
from the ST Visual Develop.
I have tried several solutions, without luck, and I suspect a OS issue.
The primary PC, is W7-64 bit, the secondary PC is W7-32bit.
Thanks
Casper Dietrich
#stm8l-discovery-64bit2011-04-10 2:12 AM
I am using STM8L Discovery on Win7 64bit.
I have same error at first. But I found solution to solve. The error is occurred when I connect one to the USB HUB. But I connect it directly to the PC. Error is not shown. Please try.2011-04-13 7:31 AM
Just an idea....
Try running STVD in a compatibility mode.
From START right click on stvd and click PROPERTIES.
On COMPATIBILITY tab try one of the various options.
2011-04-13 8:01 AM
Hi Casper,
A new ST toolset pack version will be available by 1 or 2 weeks on . It will support W7 64bit and also fix the issues encountered when trying to get the STM8L-Discovery device communicting with PCs. Best Regards