2010-03-10 07:10 AM
C file function view in STVD?
2011-05-17 06:07 AM
2011-05-17 06:07 AM
Hi,
No, that's not what I'm looking for. The workspace window in STVD (typically on the left-hand side) shows the structure of the workspace, with an expandable folder called ''Source Files'', another one for ''Include Files'', etc. What I would like to be able to do is change the view so I can expand a C file to show all functions within it. Seems like every IDE that I've used in the past has this option, but I don't think STVD does. Hopefully it will be added in future versions as it is a really handy feature.2011-05-17 06:07 AM
It was confirmed to me by an ST FAE that this is NOT an option on the current release of STVD (4.1.4).
I asked that they add it to the next release. Fingers are crossed...