STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I have customized bootloader in stm8l052c6?

Hello Respective,I am using STM8l052C6 device for my product, I want to design my own bootloader for the same.Is it possible, as I didn't find any guideline for the same in relavent documents.

NPaba by Associate II
  • 657 Views
  • 1 replies
  • 0 kudos

I would like to know how to use any timer, say TIM2, and GetCounter() correctly. I'm using SDCC on linux and compiling for an STM8L051. Please see some example blinky code. Below is the code I think should work. Any help is greatly appreciated.

void main(void) { uint16_t tmpcnt = 0; uint8_t tmpcntrl, tmpcntrh;   setup_pins();   CLK_PeripheralClockConfig(CLK_Peripheral_TIM2, ENABLE); TIM2->PSCR = TIM2_Prescaler_1; TIM2->ARRH = 0; TIM2->ARRL = 1; TIM2->CNTRH = ...

AClap.1 by Associate II
  • 1045 Views
  • 3 replies
  • 0 kudos

STM8S005K6 I2C Bus always busy

Hi.Regarding I2C Bus busy problem. I am using alternative pins (PB4 and PB5), as I have the small chip with fewer pins.Option bits are set, and verified.However even at power up the BUSY bit is set. It is set through configuration of the I2C peripher...

HMoel.1 by Associate II
  • 826 Views
  • 1 replies
  • 0 kudos

Why is the Halt() function not working?

#include <stm8l15x.h> #include <stm8l15x_pwr.h>   void main(void) { GPIO_Init(GPIOA, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOB, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOC, GPIO_Pin_All, GPIO_Mode_Out_PP_Low_Fast); ...

TheUser by Associate II
  • 2891 Views
  • 5 replies
  • 0 kudos

stm8_segment LCD problem

We are developing a product that uses segment_LCD using stm8l052r8.There was no problem when developing with com4+seg28There was a problem when developing with com8+seg24.When you turn on the entire screen, all the text on the screen comes out well.I...

0693W000001qKOBQA2.png 0693W000001qKNsQAM.png
SSHIN.11 by Associate II
  • 718 Views
  • 0 replies
  • 0 kudos

I2C Read from Slave with Python

Hi,i use a stm8s003 and SPL for programming. I am not a profi programmer.My goal is measure an Analog signal with stm8s and reading this with Python command from a Raspberry Pi.Ok, i use STM example Program I2c slave. I can read some registers from s...

Hbal.1 by Associate
  • 1125 Views
  • 0 replies
  • 0 kudos