STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to fix Cosmic Compile Error(FlexLM No such feature exists)

I want to develop an STM8 device using STVD + Cosmic Compiler.Compiler was installed with the license received by Cosmic, and the license was copied to the License folder in the Cosmic Compiler installation path (C:\Program Files (x86)\COSMIC\FSE_Com...

UHam.1 by Associate
  • 1685 Views
  • 2 replies
  • 0 kudos

STM8L050J3 SON8N - how to generate PWM on PC5 ?

Hello,I am trying to generate a PWM signal on pin PC5 using TIM2_CH1 , but no success. But I am able to generate PWM on pin PD0 using TIM3_CH2.Normally the procedure is quite simple :for TIM2_CH1 - pin PC5 TIM2_OC1Init(TIM2_OCMode_PWM1,  TIM2_OutputS...

0690X000009Yx7yQAC.png 0690X000009Yx7jQAC.png
SDomn by Associate
  • 1037 Views
  • 3 replies
  • 1 kudos

Resolved! How to read the pins map of STM8S001J3?

I have a chip with 8 pins, but I could find the start sign for pins order, should I start from left-bottom or left-upward corner?

MQi.1 by Senior II
  • 1074 Views
  • 4 replies
  • 0 kudos

What is the epilogue_w4() library call and how to stop using it?

In a function declared in RAM, I get the following warnings from the STM8 IAR compiler:Warning[Ta005]: Library call (?epilogue_w4) from within a __ramfunc function C:\myproject\src\myfiles.c 110 In the .map, I found that this function was part of vre...

GBert.2 by Senior
  • 612 Views
  • 0 replies
  • 1 kudos

Does ST still maintain the STM8 Peripheral Libraries?

For example the status of "STM8L15x/16x/05x/AL3Lx/AL31x standard peripheral library" STSW-STM8016 claims it is active. But the release notes seem to suggest that the last time someone took a look at it was at the end of 2014. That's not very active...

WilkoL by Senior
  • 1042 Views
  • 4 replies
  • 0 kudos

Multiple problems in STVD and COSMIC compiler

Hello everyone, I am using stm8l151, STVD, and cosmic compiler. I have multiple problems with STVD_STM8. Please help me as these are really confusing. I list some of them below:After I comment a line in the code, it is still active and the program st...

VYoun by Associate III
  • 912 Views
  • 1 replies
  • 0 kudos

Reset forced low

Hi, while the software are working, suddenly it will become stop, and reset pin is permanently forced low, it freaks me out!! Someone will help me, thank you so mutch

fcasa.16 by Associate II
  • 2673 Views
  • 10 replies
  • 0 kudos

Lin bus gateway using two stm8?

Hi,I need to modify data on a car's Lin bus line without generating errors on car side.I have two board with stm8 and can bus.my idea is to interrupt the car's lin bus line and connect my boards. but I don't know how to do it without affect the bus

AHaid.1 by Associate
  • 631 Views
  • 0 replies
  • 0 kudos