STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM8S SPL example on Nucleo-STM8, UART1 not working (resolved)

I am testing the STM8S Standard Peripheral Library (SPL) with a NUCLEO-8S208RB dev board. The SPL examples were written for the STM8/128-EVAL board, but can be tailored for the Nucleo. I am using the latest STVD and STVP dev tools.The SPL example 'UA...

0693W00000UnQcJQAV.png
Kmax18 by Senior II
  • 1034 Views
  • 2 replies
  • 0 kudos

Resolved! Downloading STM8S/A Standard peripheral library

I'm trying to download the standard library for the MCU stm8s003f on the ST site, but I get the message "not available for download". Is there an alternative way to get this library?

0693W00000UnWFpQAN.png
Kolab by Senior
  • 1869 Views
  • 5 replies
  • 0 kudos

Tim1 and Tim2 block each other.

Hello stm community,I am working with the STM8S001J3 processor on the ST Visual Develop Toolchain.And I use the TIM1 and the TIM2.The Tim1 is enabled via the external port when the D port is active. It is used to work synchronously with the 50hz/230v...

atürk.1 by Associate
  • 976 Views
  • 0 replies
  • 0 kudos

STM8AF Series availability

STM8A Discovery boards are NRND. Is the part discontinued/going obsolete?. According to ST, these parts are long term guarantee. 10 Year Product Longevity does not cover STM8A series.

KGane.1 by Associate III
  • 2114 Views
  • 4 replies
  • 0 kudos

How to disable POR/BOR on stm8s005k6?

I have a certain noise in my 200mV source which I believe is generating a resset in the uc. How can I disable these functions? how do i read the uc's Reset vector? Thanks.

ESopp.1 by Associate
  • 854 Views
  • 0 replies
  • 0 kudos

Resolved! ClassB STL_ClockFreqTest with HSI fails frequently on STM8AL3188

Once the STM8-SafeCLASSB SW package is integrated into our application the Periodic run time self tests are executed continuously but the STL_ClockFreqTest fails randomly. While running the entire application, that test normally fails after about an ...

RickEleo by Associate
  • 1555 Views
  • 2 replies
  • 0 kudos

I2C error handle in cosmic compiler.

Hi there.I´m using a STM8S207 with cosmic compiler.I am reading and writing a 24L64 eeprom thru i2C and everthis is working well.But i want to put protection in the routines to avoid lock the program in case of fail of a write or read command.i found...

MGarb.5 by Associate II
  • 1468 Views
  • 2 replies
  • 0 kudos