Skip to main content
debruyne.marc
Associate III
September 14, 2021
Question

ERROR IN PROGRAMMING MANUAL?????????

  • September 14, 2021
  • 4 replies
  • 4475 views

hello sir

can someone, help me with that "SUB SP,#$9 " ,with is mentioned in the LATEST PROGRAMMING MANUAL OF STM8S PAGE 151.

if you write that in an even very 1line program, you have an error

Can't match Addressing mode ' SUB SP,#$9'

is there a n error of me, or is the manual example not correct

thanks for the help

    This topic has been closed for replies.

    4 replies

    Philipp Krause
    Senior II
    September 23, 2021

    The manual looks okay to me.

    I guess you are using an assembler that uses a different syntax for hex immediates.

    You should tell us which assembler you use. E.g. in sdasstm8 (the assembler that comes with SDCC), the syntax would be sub sp, #0x09.

    Tesla DeLorean
    Guru
    July 1, 2022
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    July 1, 2022

    https://www.st.com/resource/en/release_note/rn0005-st-assemblerlinker-asm-452-lyn-319-obsend-215-stmicroelectronics.pdf

    "3.1 ASM limitations 3.1.1 Limitations for STM8 assembler �? The mnemonics of the following STM8 instructions: ADD SP,#byte SUB SP,#byte have been replaced by: ADDW SP,#byte SUBW SP,#byte"

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    debruyne.marc
    Associate III
    July 2, 2022

    hello sir

    thanks for youre answer,thats it,its works now

    a nice day