STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

finding STM8S-discovery.ht

Posted on September 27, 2010 at 19:39I want to use the RS232 example so I can figure out how to give variables to the kit and read the response but I don't have STM8S-discovery.ht.  Where do I get it? charles #cosmic #rs232

carnett1 by Associate II
  • 520 Views
  • 2 replies
  • 0 kudos

3 PWM in stm8s

Posted on September 26, 2010 at 12:39Hello All  i need use 3 pwm  by user timer1, timer2, timer3 by config TIM1_PWMIConfig(); TIM2_PWMIConfig(); TIM3_PWMIConfig(); How to config? i use stm8s-discovery #tim1 #pwm #stm8s #tim2 #timer #tim3

uthenb by Associate II
  • 699 Views
  • 0 replies
  • 0 kudos

Desoldering the sockets

Posted on August 28, 2010 at 12:18I'd like to make the board more useful by desoldering the header plugs on the board and replacing them with sockets I can plug wires directly into. I've tried using braid and my solder sucker but neither is working...

Visual Basic always return ''0''

Posted on September 20, 2010 at 13:45Hello, I'm using VB6.0 and STVP C++. C++ is no problem. But, there is some problem of VB. Always return ''0''. Our main program is only VB. not C++. Please let me know the solution of this problem.

STM8S Discovery firmware - LCD display pinout

Posted on September 15, 2010 at 22:16Hello I'm trying to connect LCD display (WH1601A) to the demo board and use firmware SPI module and SPI_SimplexLCD example as base of my code. But I can't see which PINs (ports) I should use to connect LCD displa...

STM8L UART help

Posted on September 14, 2010 at 05:52STM8L UART help

want to connect lcd to STM8S Discovery

Posted on September 01, 2010 at 14:37hi guys, recently i bought discovery and i want to connect lcd to this board. can anybody please tell me how to do that. I think code is available in examples, but i am not sure to which port lcd should be connec...

rajendra by Associate II
  • 1012 Views
  • 5 replies
  • 0 kudos