Skip to main content
infoinfo968
Associate II
August 28, 2010
Question

Desoldering the sockets

  • August 28, 2010
  • 3 replies
  • 1666 views
Posted on August 28, 2010 at 12:18

I'd like to make the board more useful by desoldering the header plugs on the board and replacing them with sockets I can plug wires directly into.

I've tried using braid and my solder sucker but neither is working effectively. Does anyone have any advice for removing these plugs ? Or am I better off using sockets and headers and so on ?

    This topic has been closed for replies.

    3 replies

    johnstrong
    Visitor II
    August 28, 2010
    Posted on August 28, 2010 at 19:33

    Paul,

    Try using a little solder on the connections first, The flux in your solder is often better than the flux on cheap desoldering wicks, also your solder will likely have a lower melting point than the boards. then use your solder puller.

    Personally, I'd leave the board along and use female jumpers, such as those made by Schmartboard.

    John

    infoinfo968
    Associate II
    August 30, 2010
    Posted on August 30, 2010 at 03:08

    Thanks - I'll look those connectors up :)

    RomainR.
    ST Employee
    September 21, 2010
    Posted on September 21, 2010 at 09:50

    Paul,

    Personally, I unsolder the 2x6 male header that I replaced by females on the copper side.

    No trouble for it with a little iron and a pump

    In this way, the board can be plug over an extension and i can access to all IO pin.

    romain

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.