Skip to main content
pierreandre
Associate III
November 11, 2013
Question

LSE crystal selection

  • November 11, 2013
  • 0 replies
  • 797 views
Posted on November 11, 2013 at 16:19

I've read the AN2867, and calculated that for having a gain margin of 5, the recommended crystal should have a max ESR of 50K and 6pF load for a minimal 3uA/V transconductance. This will not allow to use any tiny smd crystal, for example the Microcrystal CM7V-T1A.

Is there any advice about this?
    This topic has been closed for replies.