STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C peripheral (STM8S005C6) unable to detect stop event

Posted on September 05, 2017 at 22:17I2C peripheral of STM8S005C6 stop event interrupt not triggered:Using an external device (verified to be working), I generate an I2C signal (100KHz) to communicate withSTM8S005C6program as aslavereceiver with the...

0690X000006088MQAQ.png

I2C peripheral (STM8S005C6) not working

Posted on August 29, 2017 at 16:39*******************************I2C peripheral of STM8S005C6 not working******************************************I2C peripheral of STM8S005C6 does not jump to interrupt service routine:                  INTERRUPT_HA...

0690X000006083WQAQ.png 0690X000006083NQAQ.png

Problem using Touch library with STM8S003K3.

Posted on September 01, 2017 at 20:30Hello all,I am using STM8S003K3 for my appplication with STVD IDE and Cosmic compiler and using Touch Library for my application.I have added touch library in project and configure it as to work with STM8S003K3.I...

P. S. by Associate
  • 611 Views
  • 0 replies
  • 0 kudos

Beep Function in STM8S003k3

Posted on September 30, 2015 at 05:06Dear AllI have a STM8S Discovery board. I want to config PD4 with Beep function./*Initialize PD4 for beep signal */GPIO_Init(GPIOD, GPIO_PIN_4, GPIO_MODE_OUT_PP_HIGH_FAST);BEEP_Init(BEEP_FREQUENCY_1KHZ);BEEP_Cmd(...

cv-chung by Associate
  • 1155 Views
  • 2 replies
  • 0 kudos

SPI problems about STM8S103

Posted on August 28, 2017 at 10:24Good afternoon~everybodyI use STM8S103 to be the Slave device of SPI. However, I don’t know why all the interrupt of STM8 received is 0*1 instead of the right data? This is the http://www.kynix.com/uploadfiles/pdf...

STM8L Flash Programming

Posted on August 22, 2017 at 09:15I use STM8L152R8..I test flash programming... But, now some problem exists...Byte programming and word programming is no problem.But, i use block programming then CPU halted.....#pragma location = 'FLASH_CODE'void M...

STM8L151K4 Touch Sensing Problem

Posted on August 22, 2017 at 05:28I have a problem with touch sensing on STM8L151K4, It is impossibe to increase number of touch key to 12.I use sample project in STM8L_Touch_Lib and re-config the channel in 'tsl_user.h'. It work if i configure 6 ke...

Dinh Vo by Associate
  • 1011 Views
  • 2 replies
  • 1 kudos

STM8LFlash Block Programming

Posted on August 22, 2017 at 08:53I'm use STM8L152R8.I should be firmware upgrade using this cpu.But, I have some problem as below...Byte programming and word programming is no problem as belowFLASH->CR1 = 0; // Standard programming Time (EEPM, WAIT...

Write u16 to EEPROM in STM8S003F3

Posted on September 08, 2016 at 13:22 What is the right procedure to write to EEPROM? I saw the following code: oid CEEPROM::UNLOCK_EEPROM_IF_LOCKED() { if ( EEPROM_IS_WRITE_PROTECTED() ) { FLASH_DUKR = 0xAE; FLASH_DUKR = 0x56; while (...

Resolved! STM8S001 ?

Posted on July 06, 2017 at 10:08The new STM8CubeMX listed a new MCU called: STM8S001J3MxI have tried to google for it, but Ihave found Chinese only results showing demo boards too.Are there any hints when it will available for public?#stm8s001j3mx #...