STM8L101 Real Time Clock Accuracy? PPM?
STM8L101 Real Time Clock Accuracy? PPM?No info in DataSheet
Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
STM8L101 Real Time Clock Accuracy? PPM?No info in DataSheet
Is there a built in Real Time Clock in the STM8S001J3?PPM Accuracy?No info in DataSheet
i feel there should be setting for compiling larger code using full memory (64kb) and using the full 6kb ram. Can anyone guide please
Hello Every one ,I am trying to use I2c based LCD with stm8s003f3 controller. the write i2c address is 0x3f I am struck at a point ,the code is stopped in endless loop in below functionvoid PCF8574_write(unsigned char data_byte){ I2C_GenerateSTAR...
I have followed the steps to create my lin.lib file from my LDF, but I need to add it to a STVD project, not one built with an extrenal makefile. I have tried adding the library to the default compiler path, and tried specifically adding it to the pr...
The PM0044 for the STM8 MCUs explain that data address space is 16MBytes linear. Ok, so why on the page 19 data address to a RAM memory has 16-bit wide (A15...0)?
Hi everyone,I have the usual file.s19. I can set the 'Option Byte' up using the opportune tab in 'Cosmic'. Now I need to share my file.s19, but I need to share it with option byte already set up.Is there any way to do that?thanks Antonio
Posted on March 06, 2017 at 16:40Hello,Full RC5 decoding code with total STVD project file. Hope you will find it beneficial for your project.
My stm8l151k4t6 malfunctioned after I detached it from PCB in some heating way and then welded it back to the board. I wonder if the temperature I used to removed and welded the IC is too high. Anyone ever met this situation?
I have been using a STM8S105 successfully for a few months and recently, I have been experiencing problems with i/o on UART2. When I eventually probed the NRST pin I noticed that there is a sawtooth waveform on that pin, with no other circuit connect...