Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.
Hello, We had recently purchased ST-LINK/V2 Debugging and programming STM8 and STM32 microcontroller Tool and also installed ST Visual Programmer software in WINDOWS 7 PC. In our target board we are using STM8L101x3. we are not able to communicat...
Posted on May 12, 2015 at 15:57Hi,I had downloaded ''Cosmic STM8 32K Special Edition '' and had registered in: '' http://www.cosmic-software.com/download.php'' at bottom, i still didn't received the license file, what may be the problem?thanks for h...
Hello,I need to port an STM8 project to an STM32 microcontroller. The current STM8 application doesn't have any operating system and doesn't have strict time requirements: it uses only some timers for PWM signal generation, two serial interface at ve...
In STVD (ver.4.3.12 MCU: STM8L052C6)I wrote:LD A,#$68LD $5232,A ;(USART bade rate register)but memory ($5232) is $00when I wrote: LD $5000,A ;Port A data reg. memory ($5000) is $68, it work wellwhai is the different?Could anybody hel...
void sEE_Init(void) { //printf("i2c init\n"); sEE_LowLevel_Init(); // enable clock /*!< I2C configuration */ /* sEE_I2C Peripheral Enable */ I2C_Cmd(sEE_I2C, ENABLE); I2C_DeInit(sEE_I2C); /* sEE_I2C configuration after enablin...
The chip is stm8s103f3p6, and I wanna use lsi as clk and tim4 to make a timer, there are two strange things happened. when I set prescaler to TIM4_PRESCALER_4 and ARR to 32, I thought it should interrupt every 1ms (128k/4/32=1kHz), but it seems brea...
Hi,I am developing an IAP for one of my project.In that the bootloader and the application using interrupt vectors.How can I seperate the interrupt vectors for application as well as bootloader. How to relocate the interrupt vectors in STM8?T...
Hello,First off, I'd really like to thank the community for being there to help, and I really appreciate any help or guidance offered. I am trying to put an STM8S103F3 MCU into wait mode until an external interrupt on port A triggers. I make the asse...