2018-06-18 5:12 AM
The ST62 is obsolete. Is there a direct hardware replacement processor that would work in this application? Would the supplied software program for the ST62 be compatible with the new processor?
Thanks
#multiplex-lcd2018-06-18 6:01 AM
Really not sure there is any support for these 20+ year old families.
You should probably find a local ST rep or FAE and work with them to redesign/migrate the current use case, and understand your options.
You would likely need to find the source for your existing program, and recreate with current tools. A lot of DOS stuff isn't going to work at all with 64-bit Windows platforms.
An STM8 or STM32 (20-pin Cortex-M0) device should be able to driver available 7-segment displays