2018-11-30 10:12 AM
2018-11-30 11:54 AM
I found that by using the STM32CubeProg it is impossible to erase some sectors of STM32L475RG: 254, 253, 252 and so on.
2021-02-10 03:25 AM
same question here 2 years later.
I see the start address box which i cannot use?
2021-02-10 09:31 AM
2021-02-10 09:58 AM
What type of file?
A .BIN should let you set this.
A .HEX/.ELF has addresses in it, make a .BIN if you need to relocate it some place else.
2021-02-11 10:46 AM
It was a very stupid thing, i named my files as .hex instead of .bin, now i have different problems but not thisome :D