Skip to main content
pawcuq
Associate II
Dec 28, 2022 8:46 AM UTC
Solved

STM32CubeProgrammer, STM32G031K8 option bytes problem

Hello,

I have NUCLEO-G031K8 and want to change nBOOT0 using STM32CubeProgrammer (v2.12.0) but I'm unable to do so.

I get four message boxes from STM32CubeProgrammer:

  • "Warning: Option Byte: nSwap_BANK, does not exist",
  • "Warning: Option Byte: DUAL_BANK, does not exist",
  • "Warning: option Byte: DUAL_BANK, is not programmable",
  • "Option Bytes successfully programmed".
  •  

Even though the fourth message box says that option bytes were successfully programmed - nBOOT0 value is unchanged.

Here's log from STM32CubeProgrammer:

 09:41:13 : Option byte command : -ob DUAL_BANK=1 nSWAP_BANK=1 IRHEN=1 nBOOT1=1 nBOOT_SEL=1 RAM_PARITY_CHECK=1 WWDG_SW=1 IWDG_STDBY=1 IWDG_STOP=1 IWDG_SW=1 nRST_SHDW=1 nBOOT0=1 
 09:41:13 : PROGRAMMING OPTION BYTES AREA ...
 09:41:13 : Warning: Option Byte: DUAL_BANK, is not programmable
 09:41:13 : Warning: Option Byte: DUAL_BANK, does not exist
 09:41:13 : Warning: Option Byte: nSWAP_BANK, does not exist
 09:41:13 : Bank : 0x00
 09:41:13 : Address : 0x40022020
 09:41:13 : Size : 108 Bytes
 09:41:13 : Reconnecting...
 09:41:14 : Reconnected !
 09:41:14 : UPLOADING OPTION BYTES DATA ...
 09:41:14 : Bank : 0x00
 09:41:14 : Address : 0x40022020
 09:41:14 : Size : 108 Bytes
 09:41:14 : Bank : 0x01
 09:41:14 : Address : 0x40022080
 09:41:14 : Size : 4 Bytes
 09:41:14 : OPTION BYTE PROGRAMMING VERIFICATION:
 09:41:14 : Option Bytes successfully programmed
 09:41:14 : Time elapsed during option Bytes configuration: 00:00:01.199

What's strange I can change nBOOT0 using old, depreciated STM32 ST-LINK Utility (v.4.6.0).

Does anyone have a clue what I'm doing wrong?

Thanks!

This topic has been closed for replies.
Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
Dec 30, 2022 8:02 AM UTC

Hello @Community member​,

Thank you for posting,

You are doing nothing wrong, this is a bug in the latest release of STM32CubeProgrammer and is internally reported.

Internal ticket number: 139785 (This is an internal tracking number and is not accessible or usable by customers)

I apologize for the inconvenience. While programming your STM32G031 option bytes, I suggest using CLI or STM32CubeProgrammer v2.11.0.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

7 replies

Aziz BRIGUI
Aziz BRIGUIBest answer
ST Technical Moderator
Dec 30, 2022 8:02 AM UTC

Hello @Community member​,

Thank you for posting,

You are doing nothing wrong, this is a bug in the latest release of STM32CubeProgrammer and is internally reported.

Internal ticket number: 139785 (This is an internal tracking number and is not accessible or usable by customers)

I apologize for the inconvenience. While programming your STM32G031 option bytes, I suggest using CLI or STM32CubeProgrammer v2.11.0.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Houda GHABRI
ST Employee
Dec 30, 2022 9:07 AM UTC

Hi @Community member​ ,

As said by @Aziz BRIGUI​ this issue is already raised and will be fixed in next CubeProgrammer release.

Meanwhile you can use the CLI, it works fine or 2.11.0 version.

Hope this helps you.

Houda

pawcuq
pawcuqAuthor
Associate II
Dec 30, 2022 9:58 AM UTC

@Aziz BRIGUI​ @Houda GHABRI​ - thank you for quick and solid answer, I tried previous STM32CubeProgrammer version (v2.11.0) and everything works as expected :)

PS Is there any document in public which lists/describes known bugs in STM32CubeProgrammer?

Aziz BRIGUI
ST Technical Moderator
Dec 30, 2022 10:28 AM UTC

For known limitations, you can check the release notes for STM32CubeProgrammer available under this link. However since this bug is new, you won't be able to find it in that document.

I hope this helps,

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pawcuq
pawcuqAuthor
Associate II
Dec 30, 2022 10:52 AM UTC

Thank you - that's exactly what I was looking for :)

Aziz BRIGUI
ST Technical Moderator
Mar 3, 2023 8:19 AM UTC

Hello @Community member​,

Issue is resolved in latest STM32CubeProgrammer version (v2.13.0) available under this link.

Aziz

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
pawcuq
pawcuqAuthor
Associate II
Mar 9, 2023 12:17 PM UTC

Thanks :) I'll check that out.