Skip to main content
HKapo.1
Associate II
October 14, 2022
Question

STM ROM Bootloader issue with STM32H745

  • October 14, 2022
  • 3 replies
  • 1226 views

Hello,

I am facing a weird issue with accessing STM ROM bootloader for flashing.

Hardware Used: STM32H745-DISCO

IDE: Keil

I have created a simple bootloader which jumps to ROM Bootloader at startup.

startup_stm32h745xx.s:

; Reset handler
Reset_Handler PROC
 EXPORT Reset_Handler [WEAK]
				;Then check if we need to jump to ST Boot loader
 LDR R1, =0xE000ED00 ; SCB
 LDR R0, =0x1FF09800 ; ROM BASE
 STR R0, [R1, #8] ; VTOR
 LDR SP,[R0, #0] ; ROM Stack Pointer
 LDR R0,[R0, #4] ; ROM Program Counter
 BX R0	

When I power cycle and try to connect via STM32 CubeProgrammer, I get below error:

0693W00000Uo4iWQAR.png 

But when I press Reset button on STM32H745-DISCO, then connection is succesful without any issue

0693W00000Uo4j5QAB.png 

I am wondering what's the difference between pressing reset button and power cycle.

Any advice on how I can fix the issue.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
October 14, 2022

You get one shot out of reset, any noise on any of the watched pins will be taken as a connection attempt. Probably more pins moving as it powers up.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
HKapo.1
HKapo.1Author
Associate II
October 20, 2022

The STM ROM bootloader present is V9.0 and seems there is a know bug with it

0693W00000UoQs9QAF.png 

"– Additional reset needed after power off/on to enable connection to the BL interfaces"

Is there any workaround for this?

Tesla DeLorean
Guru
October 20, 2022

>>Is there any workaround for this?

Field programming, probably don't use the system's boot loader, but rather your own, using some protocol supported by standard/common tools?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..