cancel
Showing results for 
Search instead for 
Did you mean: 

ST_Link V3MINI and Cube programmer

Micisag
Associate

Dear mr.

I'm having problems with my project,

Everything was working fine, but one morning I lost connection with the target unit, see attached image.

I tried this with:

  Two ST_Link V3MINI (I got them directly from ST)

  Three different target board STM32G071 and STM32G030.

  Two different PCs.

   Two USB cable.

   Uninstall and install SW from ST.

My configuration is no RST wire.

One of the questions- My setting is "Soft reset" but in the log I see "HWrst reset mode".

I don't remember... maybe the problem started after the ST-Link update?

Please advise.

Regards

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @Micisag,

Make sure to use latest release of STM32CubeProgrammer (2.15).

Then, please keep me informed about your result.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Micisag
Associate

Hello Imen,

My target board STM32G071 start working after I've move USB cable from front my PC to rear(direct to MB of the PC)

Target board STM32G030 stay not working,

Yes, I've use latest STM32CubeProgrammer and ST-link FW.

Regards,

Micisag

Imen.D
ST Employee

Try connecting the reset pin and connect under reset mode!

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen