2025-12-09 9:22 PM
Hello
I am connecting the ST-LINK and downloading the firmware to the programmer.
I have a question. Can I do power from ST-LINK and download firmware instead of supplying external power to the MCU? Currently, I use external power, but I wonder if there is such a way.
Thank you.
Solved! Go to Solution.
2025-12-09 10:39 PM - edited 2025-12-09 10:41 PM
Hi,
A genuine st-link has no power output, so no power for the target.
Only if you solder/wire a connection to get power yourself, let say with a st-link V3 mods, you can have some 100mA or so from the st-link. See the manual for st-link V3mods.
2025-12-09 10:39 PM - edited 2025-12-09 10:41 PM
Hi,
A genuine st-link has no power output, so no power for the target.
Only if you solder/wire a connection to get power yourself, let say with a st-link V3 mods, you can have some 100mA or so from the st-link. See the manual for st-link V3mods.
2025-12-10 1:17 AM
You didn't say what ST-Link you're using - there are several versions:
TN1235: Overview of ST-LINK derivatives
Those are the real ones; there are also fakes/clones - see: How to recognize a genuine ST-LINK/V2 versus a cloned one.
The User Manual for the particular model you have will describe its capabilities...
2026-01-13 7:26 AM - edited 2026-01-13 7:26 AM
Hi @giwonKIM,
Along with comments said by @Andrew Neil and @AScha.3, there's also the STLINK-V3PWR that can power the STM32.
If any of these answers address your question, please mark the comment as accepted solution.
Thanks in advance,
Aziz