Not able to connect with stm32 cube programmer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-28 10:44 AM
Dear sir,
I want to connect my stm32 board with stm32 cube programmer. ​but there is some issue,
1.i am able to read the device number , but the connect led does not turn green
2. Then I get messages of check boot configuration and serial port.
3. I tried keeping the boot pin high at the time of reset , so as to take the Mcu in bootloader mode. , but it did not help.
4. Please suggest
​
Thanks
Rgds
Nikhil ​
- Labels:
-
STM32CubeProgrammer
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-28 11:26 AM
What STM32?
A board you designed?
Schematics?
Connectivity?
Assuming connecting via serial, PC side COM port. What type of serial connection, the STM32 outputs/expects CMOS levels, not RS232.
Make sure the RX/TX for each end of the connection are appropriate, ie the output of one device goes to the input of the other.
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
‎2022-08-01 11:42 PM
Dear Sir,
I am using STM32L476 controller and i am using STM32 Cube programmer to communicate with the board using UARTterminal
1) i power on the device, then keep the BOOT pin high and then release the boot pin , but i do not get the green Connect LED in the Application, the hardware wires are properly connected to each other,
in the STM32 cube programer i get the following details
12:04:55 : Serial Port COM4 is successfully opened.
12:04:55 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
12:04:57 : Timeout error occured while waiting for acknowledgement.
12:04:57 : Activating device: OK
12:04:57 : Board : --
12:04:57 : Chip ID: 0x415
12:04:57 : BootLoader protocol version: 3.1
12:04:57 : Response received from device: NACK
12:05:00 : Error: RDP is set to level 1, try using Read UnProtect (-rdu) command in order to remove the Read Out Protection.
12:05:00 : UPLOADING OPTION BYTES DATA ...
12:05:00 : Bank : 0x00
12:05:00 : Address : 0x1fff7800
12:05:00 : Size : 40 Bytes
12:05:00 : Response received from device: NACK
12:05:00 : Error: READ command not acknowledged at address: 0x1FFF7800
12:05:00 : Error: Uploading Option Bytes bank: 0 failed
12:05:00 : Error: Initializing the Option Bytes failed
12:05:00 : Disconnected from device.
12:05:29 : RTS low
12:05:29 : DTR low
12:05:29 : Serial Port COM4 is successfully opened.
12:05:29 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
12:05:31 : Timeout error occured while waiting for acknowledgement.
12:05:31 : Timeout error occured while waiting for acknowledgement.
12:05:31 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
i am able to program the board using another discovery board.
Please suggest
thanks
nikhil