2021-08-29 10:06 AM
I'm running Ubuntu 21.04 and have set the env variable to force use of X11:
GDK_BACKEND=x11The utility runs and can discover connected ST-Link devices, but when I click connect button the tool crashes in the connectStLink function:
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007f2873aa90a3, pid=64882, tid=0x00007f2862a73640
#
# JRE version: OpenJDK Runtime Environment (8.0_265-b01) (build 1.8.0_265-b01)
# Java VM: OpenJDK 64-Bit Server VM (25.265-b01 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libCubeProgrammer_API.so+0x500a3] connectStLink+0x293
Solved! Go to Solution.
2021-11-23 11:33 AM
Java: write once, crash everywhere.
I've seen problems with 2.8.0 (ST-LINK firmware is up-to-date) crashing when attempting to connect while the target processor is being held in reset. I believe earlier versions would just complain but 2.8 catches fire. Progress!
2021-12-08 6:46 PM
Only solution for me on Ubuntu 21.04 is to remove whole directory of STM32CubeProgrammer then install 2.7.0 then it works.
2021-12-14 7:49 AM
The solution to this problem was found installing the STM32CubeProgrammer v.2.7.0 and trying to connect. The message was "Error: Unable to list supported devices", and the solution is to run the application from inside the "STM32CubeProgrammer/bin" folder. The only difference with v.2.9.0 is that the application gets out, but the error is the same.
You only need to add the instruction "cd $DIR" in the file "STM32CubeProgrammer/bin/STM32CubeProgrammer" as showed bellow:
#!/bin/bash
DIR="$( cd "$( dirname "${BASH_SOURCE[0]}" )" && pwd )"
export LD_LIBRARY_PATH=$DIR/../lib:$LD_LIBRARY_PATH
cd $DIR
$DIR/jre/bin/java -jar $DIR/STM32CubeProgrammerLauncherIf the application don't connect yet, you must connect with the option "Reset mode : Hardware reset".
I tested with 3 boards with ST-Link v.2.1 and v.3.0 and all connected.
Good luck!
2021-12-16 6:42 AM
In my case, a Blue Pill board, I had to press and hold its reset button to get it connected...
2021-12-23 9:26 AM
I can confirm that 2.8.0 simply crash when the "Connect" button is pressed and the ST-Link is without any MCU connected to it. If there is an MCU connected to the ST-Link it works normally.
Tested with Linux Mint 20.2 and a clone ST-Link V2 dongle with an old FW (ST-LINK FW : V2J34S7).
Regards
2021-12-25 9:35 AM
The same for me. Crashes during the connect. v 2.9.0
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x00007faaa89f8281, pid=66190, tid=0x00007faa581fb700
#
# JRE version: OpenJDK Runtime Environment (8.0_265-b01) (build 1.8.0_265-b01)
# Java VM: OpenJDK 64-Bit Server VM (25.265-b01 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libCubeProgrammer_API.so+0x73281] GetDeviceGenInf(TargetInterface*)+0x21
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# If you would like to submit a bug report, please visit:
# http://bugreport.java.com/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
2022-02-27 9:41 AM
Still the same error.
2022-03-02 2:37 AM
Hello @SFuch.1 ,all,
Thanks for your feedbacks.
I confirm there is issue with the new Version of Ubuntu 21.10 , it is already raised internally and fixed.
The fix will be available in the next CubeProgrammer version 2.10.0 scheduled soon.
Internal ticket number: 115515 (PS: This is an internal tracking number and is not accessible or usable by customers).
Houda
2022-04-27 2:35 PM
Edit: I am working with an MPU and have just discovered the prgorammer does not support swd interface for mpu. I would however suggest that the program should'nt crash.
I am running version 2.10.0 and am running into the same problem. Has this been addressed in 2.10.0 or are we still waiting for a patch?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.