2024-06-27 4:07 AM
good morning, i am using stm32h747i-disco board. for that when i am executing Touchgfx generated file into stm32cubeide. i am able to debug the m4 processor but not m7 processor. i am getting an error with " internal .elf file".
then i did cm7 processor to off in stm32cubeprogrammer and executed the code. from then i am not able to debug the cm4 and cm7 processors, and i am not able connect the cube programmer. and yes i have upgraded the firmware. any help would be so appreciated. thank you in advance.
2024-07-16 6:54 AM
Hello @suhfi
You might have chosen the wrong power mode for your board. This might explain why you're unable to connect to the target anymore. I suggest checking this link : How to unbrick an STM32H7 after setting the wrong ... - STMicroelectronics Community.
Let me know if you find this helpful.
Aziz