cancel
Showing results for 
Search instead for 
Did you mean: 

External loader issue with STM32H743 and W25Q256

mtechmatt
Associate III

Hi,

I am using Clives loader for the STM32H with the correct pins etc but it never works in the STM IDE, so I thought I would follow controllertechs videos to try and make my own loader, that didn't work either, but I did verify all the QSPI parts reading/wriitng etc are working. I also learned a good test using the CubeMX Programmer (and that fails using my loader for a different reason) but, I then thought OK will test it with Clives and MX Prog, and that fails on verification when I try and load a 1MB test file. I have emailed Clive and he has been incredibly helpful already, but thought I would also ask in the community in case someone has a quick solution?

mtechmatt_0-1725012574894.png

 

 

13 REPLIES 13

@mtechmatt wrote:

Mem protecctino was the issue!!]

 

 What do you mean by "Mem protecctino"? memory protection?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Hi Soflt I updated my original post. The key thing is to turn off the MPU.

Hi mtechmatt,

could you try to attach a zip file ?

I just wrote a loader and it's working, but I would just like to do a bit of comparison...

 

Thanks,

regards

 

Lucio

...message moved in a new thread:

external loader issue with stm32h743 and w25q512 

Thanks!