cancel
Showing results for 
Search instead for 
Did you mean: 

Why NUCLEO-H753 ADC channel 12 is missing in CubeMX

PeterWangPTD
Associate II

Hi,

    Why NUCLEO-H753ZI ADC channel 12 is missing in CubeMX ?

     ADC channel 12 is in NUCLEO-H753ZI board CN9-9 connector.

     A few other ADC channels are also missing in CubeMX.

    Thanks,

 

Rong

11 REPLIES 11

"I've already posted the Nucleo with that package doesn't have channel 12. " - yes - because PC2 should be PC2_C, which does not exist in this board.

Thanks

lol, It's over your head. 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source