cancel
Showing results for 
Search instead for 
Did you mean: 

Why CubeMx doesn't support DP83848 in RMII mode ?

Peko
Associate III

Hi,

I need create UDP server on STM32F407 with PHY DP83848 in RMII mode. I started with CubeMx, but it support only LAN8720 in this mode.

What is the solution?

Thank you.

Peter

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Nawres GHARBI
ST Employee

Hi @Peko​ 

Thanks for the feedback it will be fixed for the 5.1.0

Hi,

the actual version is 4.27. When you plan to release version 5.1.0 ?

What are the differences between LAN8720 and DP83848 in RMII mode?

Peter

Hi @Nawres GHARBI​ 

I have tried release version 5.5.0 and this issue still exists. I can see DP83848 as a dropdown option in MII mode only, and LAN8720 as an option in RMII mode only. I am using DP83848 in RMII mode. When do you expect this to be fixed?

@Peko​ Did you resolve this? Would you be willing to share your CubeMX project and/or code changes?

Matthew.