USB device MSC is too slow to access an SD in FAT32 (it works fine with FAT)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 3:30 PM
Hi to all,
I use the Device MSC provided by CubeMX.
I wrote my own diskio.c file and every works fine with an SD of 2Gb formatted in FAT.
When I use n SD of 8Gb formatted in FAT32, WIndows take about 2 minutes to access the root directory. After this time, the Mass storage works fine.
What is the delay in enumerating files in FAT32?
Attached my usbd_storage_if.c
P.S.: FATFS works great with the same user_diskio.c and user_spi_diskio.c (attached)
Thanks to all.
- Labels:
-
STM32CubeMX
-
USB
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 3:57 PM
Well USB-FS isn't exactly particularly fast, FAT 32 and EX structures are quite large, and these can be particularly slow on SD Cards if you've just random formatted them, and ignored the erase block sizes, and alignment issues.
MSC will get bogged down if you only allow for a single sector access, this has a massive overhead for SD Cards. Ideally you want to be doing 32KB or entire clusters at a time.
Check there's a MSC_PACKET_SIZE type variable, and it doesn't want to be ONE
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 6:04 PM
usbd_conf.h
/* MSC Class Config */
#define MSC_MEDIA_PACKET (8 * 1024)
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 10:17 PM
Hi TD,
I try
#define MSC_MEDIA_PACKET (8 * 1024)
but still remain the issue. The strange thing is that after 2/minutes, the access on SD works fine, it is only the first phase that is very slow.
looking for some other parameter, Ifind this two in usbd_msc.h:
#define MSC_MAX_FS_PACKET 0x40U
#define MSC_MAX_HS_PACKET 0x200U
what are the difference between this parameter ?
Can I increase FS_PACKET to 0x200 ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-17 10:07 PM
MSC_MAX_FS_PACKET is inside an uint8_t array. So increase it is not a solution for my problem
__ALIGN_BEGIN uint8_t USBD_MSC_DeviceQualifierDesc[USB_LEN_DEV_QUALIFIER_DESC] __ALIGN_END =
{
USB_LEN_DEV_QUALIFIER_DESC,
USB_DESC_TYPE_DEVICE_QUALIFIER,
0x00,
0x02,
0x00,
0x00,
0x00,
MSC_MAX_FS_PACKET,
0x01,
0x00,
};
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-21 9:46 AM
I made some other test.
once the Mass storage is opened in Windows, reading is pretty good, but writing is very difficult.
I think that I have to change low level routine to obtain a good USB troughput.
I try to adapt the example.
I'll let you know how it goes
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-21 11:22 AM
SPI isn't exactly the fastest way. Most use the SDIO/SDMMC peripheral to get tens of MBps rather than the few hundred KBps you're likely working with.
Benchmark the underlying IO routines, this will give you a better understanding of the bandwidth you've got to play with, and whether the USB side is terribly impactful on the whole speed issue, or not.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-26 3:12 PM
Hi, I come back to the subject after several tests.
I have achieved decent speed with SPI and DMA (although only transcend brand SD cards support DMA), but the slowness remains.
Through wireshark I captured the USB enumeration both with the STM32 and with a USB-SD converter (using the same SD): the difference lies in the wMaxPacketSize parameter which in the STM32 is 64, while in the converter it is 512 ( attached photo).
How to configure the size of the data packet in the USB device (it seems to have been done: here)
I tried to change the fields
#define USB_FS_MAX_PACKET_SIZE 64U
#define USB_MAX_EP0_SIZE 64U
but different values ​​cause incorrect enumeration on the PC.
The MSC_MAX_FS_PACKET field appears not to be used (by changing the name, compilation occurs without errors).
Can you give me indications on the increase of the data package?
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-09-26 3:34 PM
Bus packets on the USB are separate from those on the SD card interface, single sector interactions on the SD card have very large overheads, which diminish significantly when large blocks, perhaps whole clusters, can be read in a single interaction.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-11 2:53 PM
The theory is chira, I needed some clarification on how to increase the packet size.
Changing the parameter MSC_MAX_FS_PACKET has no effect.