cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L432 UART receive IRQ handler unable to created by Cube

LU998
Associate II

Hi, guys, anyone has met such an issue?

I was trying to generate code by CubeMX, and I also wanna generate USART1 IRQ handler but failed.

here are my settings, anyone can help me with this?

LU998_2-1713429216523.png

thanks

LU998_0-1713429145150.png

LU998_1-1713429167470.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

Umm, no. It's in stm32l4xx_it.c file.

But you shouldn't need to do anything in that file anyways. All your coding would be done in the callbacks which are in stm32l4xx_hal_uart.c or stm32l4xx_hal_uart_ex.c. You just override the weak callbacks that you want to use.

CANable V3 firmware | CAN-X CAN bus analyzer software for CANable V3 |
TimerCallback tutorial! | UART and DMA Idle with multiple UART instances tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

View solution in original post

4 REPLIES 4
Karl Yamashita
Principal

Are you looking at the correct file where it gets generated?

CANable V3 firmware | CAN-X CAN bus analyzer software for CANable V3 |
TimerCallback tutorial! | UART and DMA Idle with multiple UART instances tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

the IRQ handler should be at main.c ?

 

Umm, no. It's in stm32l4xx_it.c file.

But you shouldn't need to do anything in that file anyways. All your coding would be done in the callbacks which are in stm32l4xx_hal_uart.c or stm32l4xx_hal_uart_ex.c. You just override the weak callbacks that you want to use.

CANable V3 firmware | CAN-X CAN bus analyzer software for CANable V3 |
TimerCallback tutorial! | UART and DMA Idle with multiple UART instances tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
LU998
Associate II

thanks anyway