cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7, STM32F7 cache enabled and MPU disabled

BVu
Associate III

I'm using STM32H723, and STM32F767. CubeMX allows the data cache to be enabed and leave MPU disabled. Is this a valid configuration? Yes, i do know how to configure the MPU. Am i required to enable the MPU and configure all regions to have same attributes if i simply want the whole SRAM to be cacheable?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

> CubeMX allows the data cache to be enabed and leave MPU disabled. Is this a valid configuration?

Yes.

> Am i required to enable the MPU and configure all regions to have same attributes if i simply want the whole SRAM to be cacheable?

No. SRAM is write-back write-allocate cached by default (at least on the H7). You can use the MPU to override this, but don't have to.

https://www.st.com/resource/en/application_note/dm00272913-level-1-cache-on-stm32f7-series-and-stm32h7-series-stmicroelectronics.pdf

0693W000006HUaCQAW.png

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

> CubeMX allows the data cache to be enabed and leave MPU disabled. Is this a valid configuration?

Yes.

> Am i required to enable the MPU and configure all regions to have same attributes if i simply want the whole SRAM to be cacheable?

No. SRAM is write-back write-allocate cached by default (at least on the H7). You can use the MPU to override this, but don't have to.

https://www.st.com/resource/en/application_note/dm00272913-level-1-cache-on-stm32f7-series-and-stm32h7-series-stmicroelectronics.pdf

0693W000006HUaCQAW.png

If you feel a post has answered your question, please click "Accept as Solution".