STM32G031F8P6 Startup Problem with CubeMX generated code SysTick on Timer16
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-10 2:41 AM
I seem to be having issues with a basic CubeMX generated setup on my G0 board. I seem to end in nowhere land after any timer interrupt takes place, when i stop the debugger i am somewhere around (0x1fff1xxx)
Even if try to run a basic timer setup with CubeMX doing all the code generation for SysTick on timer 16. As soon as the TIM16 interrupt is enabled in HAL_Init after it setups the timer this happens a random number of few instructions afterwards.
Everything looks OK on the surface.
-Fresh CubeMX setup. Default interrupt table location.
-Bootmode0 is pulled low with 10k resistor (Flash boot)
-Interrupt table has .word TIM16_IRQHandler /* TIM16 */
-I have void TIM16_IRQHandler(void) to catch it
HAL Init seems to set up the clock for the periheral, settings, etc.
What am i missing?
- Labels:
-
STM32CubeMX
-
STM32G0 Series
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-10-10 4:31 AM
I have verified the vector table looks correct. The address of TIM16_IRQHandler appear in the correct spot in the vector table.
As extra information i am running with the internal RCs without external crystals.
Once the event has happened the priority mask is 0x1
SP : 0x20000e38 (valid place i think)
PC: 0x1fff11ec (somewhere in flash, i would expect 0x800xxxxx right?)
basepri, faultmask, control is 0
Any ideas?