Associate
February 11, 2017
Question
STM32F4 HAL SPI NSS won't work with baudrates below 1 MBaud
- February 11, 2017
- 2 replies
- 1373 views
Posted on February 11, 2017 at 19:50
Hi,
I'm trying to set up a SPI connection for an AS5311 sensor on my STM32F I want to use the hardware controlled NSS signal, which is working pretty well - but only for high baudrates.
I am using CubeMX to configure my clocks and peripherals. If I set the baudrate above 1 MBaud and read the sensor data with the
HAL_SPI_Receive_IT(...) function the NSS signal is used properly. But if I change it to a baudrate below 1 MBaud, NSS is not working anymore. I do not change anything on my source code. I olny use the prescaler setting for SPI in CubeMX.
Does anyone know the reason for this? Unfortunatly the sensor does not support baudrates above 1 MBaud. See the pictures below to comprehend my problem
#hal #cubemx #baudrate #nss #nss-cs #spi