cancel
Showing results for 
Search instead for 
Did you mean: 

STM32cubeMX USB_DEVICE Middleware - Optimum Parameter setting guide line

mahapusha
Associate III

Dear Members,

Is there any guidelines to select the values or size of three parameters in STM32cubeMX, middleware (USB device, CDC) to achieve the highest speed on CDC? I am using STM32L4P5VGT. My application streams the sensor data to the Laptop using USB CDC class, once powered on.

To understand the question more in detail, I attached my current settings, are acceptable or can be optimised by reduction or increase, same time, need to avoid wastage of RAM also, so it can be used for other purposes if I am using too much.
Regards

 

0 REPLIES 0