cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 6.7.0 released

Semer CHERNI
ST Employee

We are pleased to announce you that the official release of STM32CubeMX v6.7.0 is available for download here

What is new in STM32CubeMX V6.7.0?

  • New CPNs: STM32WL STM32WL5MOCHx
  • Boards:
    • STM32WB STEVAL-PROTEUS1 
    • STM32F0 STM320518-EVAL
    • ST32WL B-WL5M-SUBG1
  • "CAD Resources" support in CubeIDE
  • I-Cube "MadeForSTM32" examples description generation
  • STM32L5: Cohabitation CubeAzure USBX (pack) & UCPD (MW)
  • STM32F7 and STM32F4: Both ETH_RX_BUFFER_SIZE and ETH_RX_BUF_SIZE constants are specifying the size of the same buffer
  • MWs upgrade:
    • TouchSensing v2.2.8 for WB
    • USB Device Lib v2.11.1 for L5, WB and H7
    • USB Host v3.5.0 for H7
    • USBPD Library v4.1.0 & device l5_v5.0.0 for L5
    • USBPD Device v3.4.1 for G0
    • Open Thread 1.3 for WB
    • KMS v1.1.9 for WL

Main fixed issues

130537 [Project Manager] Wrong call order for MDMA/DMA Init functions

119809 [MX-L5][CodeGen] Warning generated when IP initialization as a pair of .c/.h

125698 [Cortex-M7] No default MPU configuration is proposed

126668 [MX-HRTIM][LL] Issue in HRTIM init in LL code when "General peripheral initialization as a pair of .c/.h files per peripheral " parameter is checked

128892 [IDE-GUI][H7]Changing MDMA list type from linear to loop listing causes MX tab to appear * even after saving modification

131802 [MX-CodeGen][H7] Project showing error during generation after enabling multi-threaded support checkbox for cortexM7

132093 [DMA] MX_DMA_Init() is called after MX_TIM23_Init()

133163 [STM32CubeMx] [DRR] DDR3 settings unavailable using STM32CubeMX

134921 [HRTIM] HRTIM generated code that enable Resynchronized Update even we disable it

134934 Execution in RDP-2 impacted by DWT-based code in SystemClock_Config()

135590 [MX-ETH][MW-LWIP] HAL_ETH_Start should be replaced with HAL_ETH_Start_IT in "ethernet_link_thread" function

137342 [STM32CubeMx] [FreeRtos] The tool can't open the *.ioc file if user constants are used with FreeRtos

138331 Issues with toolchain location folder and Makefile toolchain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
JAgue.1
Associate II

Hi everyone,

Since the update my CubeMX has been in troubles:

  • It's stopping the generation randomly and force me to kill the task
  • It is forgetting code part and some configuration in the linker

I'm working on a stmf7xx with FreeRTOS activated, even if i'm pretty confident that is not related to my issues.

I will try to downgrade to 6.6.X.

eg7963
Associate III

Yeah well,

I updated my STMCubeMX installation and, at the very end, the application froze once the update window closed, then the exe of the app also disappeared from my HD (again) and now i can just perform another installation from the start (again).

I thought that problam had been addressed and solved already years ago, as it was already the case in the past, but apparently, the problem is still here.

SErbo
Associate

Am I the only one who cannot unzipped the downloaded file? 7zip and winrar tell that the file is corrupted. the error come up in each version of setup.