2023-10-30 9:51 AM
Hi all,
I'm using STM32Cube IDE (version 1.13.1, build 17479_20230728_0839 ) to manage my company project based on a STM32U5 MCU.
More specifically, I'm using linked list feature (for playing audio with SAI + DMA transfer) and I have noticed what appears to me as a bug in auto-generated code.
Basically, I have created through CubeMx one list named SAIQueue, with one node named NodeTx and the auto-generated initialization code is the following:
/**
* @brief DMA Linked-list SAIQueue configuration
* @PAram None
* @retval None
*/
HAL_StatusTypeDef MX_SAIQueue_Config(void)
{
HAL_StatusTypeDef ret = HAL_OK;
/* DMA node configuration declaration */
DMA_NodeConfTypeDef pNodeConfig;
/* Set node configuration ################################################*/
pNodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
pNodeConfig.Init.Request = GPDMA1_REQUEST_SAI1_B;
pNodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
pNodeConfig.Init.Direction = DMA_MEMORY_TO_PERIPH;
pNodeConfig.Init.SrcInc = DMA_SINC_INCREMENTED;
pNodeConfig.Init.DestInc = DMA_DINC_FIXED;
pNodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
pNodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
pNodeConfig.Init.SrcBurstLength = 1;
pNodeConfig.Init.DestBurstLength = 1;
pNodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
pNodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
pNodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
pNodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
pNodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
pNodeConfig.SrcAddress = 0;
pNodeConfig.DstAddress = 0;
pNodeConfig.DataSize = 0;
/* Build NodeTx Node */
ret |= HAL_DMAEx_List_BuildNode(&pNodeConfig, &NodeTx);
/* Insert NodeTx to Queue */
ret |= HAL_DMAEx_List_InsertNode_Tail(&SAIQueue, &NodeTx);
ret |= HAL_DMAEx_List_SetCircularMode(&SAIQueue);
return ret;
}
If I run this code without modification, I encounter an assert failure in HAL_DMAEx_List_BuildNode (line 1069 of file stm32u5xx_hal_dma_ex.c):
assert_param(IS_DMA_MODE(pNodeConfig->Init.Mode));
This is fixed by adding the following missing line in "pNodeConfig" structure initialization:
pNodeConfig.Init.Mode = DMA_NORMAL;
Obviously, if I do any modification on the ioc file and relaunch code generation, this line is deleted and the issue is back.
Am I missing something on the UI to generate this line properly? Should this be fixed?
Thanks in advance for any insights.
2024-08-23 8:56 AM
Hello @fsorin & thanks for your post.
I have also just hit the same problem with STM32CubeIDE 1.16.0 and STM32CubeMX 6.12.0-RC9.
In my opinion the code relies on pNodeConfig being initialised to all 0's (which it is not because it is a stack variable) before the node configuration is set.
My solution was to make an local copy of MX_SAIQueue_Config() which clears first clears pNodeConfig before setting the other values.
It would be nice if ST could fix this auto-generation bug. Note my function has an Ex() suffix...
#include "linked_list.h"
extern DMA_NodeTypeDef NodeTx;
extern DMA_QListTypeDef SAIQueue;
static HAL_StatusTypeDef MX_SAIQueue_ConfigEx(void)
{
HAL_StatusTypeDef ret = HAL_OK;
/* DMA node configuration declaration */
DMA_NodeConfTypeDef pNodeConfig;
#if 1
// Bug fix
memset(&pNodeConfig, 0, sizeof(pNodeConfig));
#endif
/* Set node configuration ################################################*/
pNodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
pNodeConfig.Init.Request = GPDMA1_REQUEST_SAI1_A;
pNodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
pNodeConfig.Init.Direction = DMA_MEMORY_TO_PERIPH;
pNodeConfig.Init.SrcInc = DMA_SINC_INCREMENTED;
etc...
2025-12-02 7:15 AM
I had the exact same issue with the STM32U5GF8, GPDMA, Linked-Lists and MX generated code, without this line it won't work,
pNodeConfig.Init.Mode = DMA_NORMAL;Thanks to all who took the time to solve these issues and post the solutions.