2021-06-03 5:48 AM
While setting up a project using cubeMx for a stm32G0, I stumbled across a possible error on the USB_device files. This error resulted in the usb reset handler stalling the machine. My project specifies the USB as full speed and looking in the generated usbd_conf.c, I found the following lines in HAL_PCD_ResetCallback
USBD_SpeedTypeDef speed = USBD_SPEED_FULL;
if (( hpcd->Init.speed != USB_DRD_SPEED_FS) || (hpcd->Init.speed != USB_DRD_SPEED_LS))
{
Error_Handler();
}
/* Set Speed. */
USBD_LL_SetSpeed((USBD_HandleTypeDef*)hpcd->pData, speed);
/* Reset Device. */
USBD_LL_Reset((USBD_HandleTypeDef*)hpcd->pData);In that case the line 2 test will always result in the Error_handler being called as we are indeed FS (and thus not LS). Using thins condition instead solved the usb issue :
if( hpcd->Init.speed != USB_DRD_SPEED_FS){
Error_Handler();
}Could this be an oversight in the cubeMX generation or is it that I missed something blatantly obvious ?
Solved! Go to Solution.
2022-02-15 7:44 AM
I am using stm32cubemx 6.4.0 with the fixed version of HAL_PCD_ResetCallback, but still can't get usb device to work.
I created template project by cubemx, and selected usb cdc device from middleware and enabled usb in connectivity. I also enabled swd for debug.
I solved clock in wizard, hclk is clocked from hsi16->pll, and usb clock is hsi48.
after rebuild and download, device triggered a enumeration but doesn't reply to host.
I am using a beagle usb sniffer, it doesn't reply first setup packet(get descriptor).
the dfu bootloader works fine if I erased flash, so it's not a hardware problem I think.
edit:
I changed some extra options in cubemx, if I enable CRS sync in RCC settings and usb interrupts in NVIC settings, usb device can be recognized by host now.
2022-02-15 8:27 AM
Oh, now you find it. I was on the way to write this:
I have not used that version, but maybe I anyway can recommend to check that the "USB, UCPD1 and UCPD2 global interrupts" is enabled, (System Core - NVIC).