cancel
Showing results for 
Search instead for 
Did you mean: 

Missing enum values for STOP2_MODE in system_debug_signal_t cause compilation error

lgc
Visitor

I am configuring to support Stop mode 2 in the stm32_wpan configuration section in the STM32CubeMX.

The following lines are generated in stm32_lpm_if.c

SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_ENTER);
SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_ACTIVE);
SYSTEM_DEBUG_SIGNAL_SET(LOW_POWER_STOP2_MODE_EXIT);

However, the definitions of LOW_POWER_STOP2_MODE_ENTERLOW_POWER_STOP2_MODE_ACTIVE and LOW_POWER_STOP2_MODE_EXIT don't get generated, which are causing undefined compilation errors.

I checked the expected types for these definitions, and see that these should be defined as part of the system_debug_signal_t enum inside debug_signals.h. I have tried looking for additional configurations that might generate the missing definitions but I haven't had any success so far.

What should I look into or how can I generate these missing definitions? I could try to manually add these definitions to system_debug_signal_t. but then any time I re-generate with new configurations it will get ovewritten.

I am using STM32CubeMX version 6.14.0  

Toolchain: EWARM V9.20

MCU Reference:STM32WBA63CIUx.

Firmware package name and version: STM32Cube FW_WBA V1.6RC2

The project uses the STM32_WPAN and X-CUBE-FREERTOS software packs, currently trying to set the following configurations in STM32_WPAN:

CFG_LPM_LEVEL = 2

CFG_LPM_STDBY_SUPPORTED = 2 (for Stop mode 2)

1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @lgc 

First let me thank you for posting.

I would appreciate it if you could provide your IOC so that I can check the configuration and further investigate.

THX

GHofrane