cancel
Showing results for 
Search instead for 
Did you mean: 

Maybe a bug on cubemx for F3

paolovasta9
Associate II
Posted on August 10, 2014 at 00:05

Maybe a bug on cubemx for F3

#cubemx-stm32-nmi-headler
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on August 10, 2014 at 15:09

The forum does not work from mobile/tablet devices, please try again.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
paolovasta9
Associate II
Posted on August 10, 2014 at 16:41

Ok sorry.

I tryed to create a project for STM32F302R8 with SPI and interrupt with CubeMX. Everything appeared to be good but when I tryed to use the function HAL_SPI_Transmit_IT the firmware went to NMI_Handler error. After some test I understood that in the project there wasn't the startup_stm32f302x8.s file. I put this file manually and all work fine. I think that this is an error from CubeMX because when i generate a code for STM32F4 this file is automatically included.

Hope to help somebody..

Paolo Vasta

stm32cube-t
ST Employee
Posted on October 06, 2014 at 16:25

Hello, we can not reproduce your issue. Can you indicate which version of CubeMX you are using and which toolchain (EWARM, MDK-ARM, or TrueStudio).

Thank you