Is it possible to fully automate the creation of a * .ioc file from a script (STM32CubeMX -q script.txt)?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-21 6:25 AM
Rationale:
I have several projects on the same MCU that evolve almost simultaneously. (However, the pinout is different). When adding new features, I have to enable some of them in GUI mode several times. `sort`ing the contents of *.ioc files alphabetically and `diff`/merging helps in part.
Is it possible to fully automate the creation of a * .ioc file from a script (STM32CubeMX -q script.txt)?
script.txt:
swmgr install stm32cube_h7_1.9.0 accept
load STM32H743VITx
project name M7_MODBUS
project toolchain SW4STM32
SetStructure Advanced
SetCopyLibrary "copy only"
project couplefilesbyip 1
# Working, ip "CORTEX_M7" available
set ip parameters CORTEX_M7 CPU_ICache Enabled
set ip parameters CORTEX_M7 CPU_DCache Enabled
# Not working. How to click "Activated" checkbox (enable) on IWDG1 via this script?
set ip parameters IWDG1 Reload 4000
set ip parameters IWDG1 Window 4000
Labels:
- Labels:
-
STM32CubeMX
-
STM32H7 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0