Flash problem (original STLINK & IC from DigiKey)
I am getting this error, while the setup in cubemx is for this chip... Using SW4STM32.
Wrong device detected, check your project and the board(s) connected
Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
none separate
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 4000 kHz
adapter_nsrst_delay: 100
Info : clock speed 4000 kHz
Info : STLINK v3 JTAG v1 API v3 SWIM v1 VID 0x0483 PID 0x374F
Info : using stlink api v3
Info : Target voltage: 3.309742
Info : Unable to match requested speed 4000 kHz, using 3300 kHz
Info : Stlink adapter speed set to 3300 kHz
Warn : UNEXPECTED idcode: 0x0bc11477
Error: expected 1 of 1: 0x2ba01477
in procedure 'program'
in procedure 'init' called at file "embedded:startup.tcl", line 495
in procedure 'ocd_bouncer'
** OpenOCD init failed **
shutdown command invoked