cancel
Showing results for 
Search instead for 
Did you mean: 

Error downloading FW.F1.1.7.0 MCU package

Dmitri
Associate II

Hi,

recently I installed STM32CubeMX. When I click 'Check for update' menu item 'STM32CubeF1 Firmware Package V1.7.0 / 09-October-2018' is shown. But when I press 'Install Now' the following error happens:

In the log I see:

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:919 - Problem, file not found on Server

2018-11-20 23:56:39,197 [ERROR] ServerAccessManage:491 - Problem, file not found on Server : stm32cube_fw_f1_v170.zip.

Is v1.7.0 package available to download?

thanks,

Dmitri

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
LOVEKUSH PRATAP
Associate II

I'm still getting this error

error downloading the following files: stm32cube_fw_f1_v170.zip(cannot unzip) stm32cubemx

Well the .ZIP should be in the Repository, you can Check/Test it with something like WinRAR.

More critically the system will fail this way if your hard drive is out of space. Figure you're going to need more than 3.6 GB free to download and unpack

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Hello. Faced a similar problem.

error downloading the following files: stm32cube_fw_f1_v170.zip

When will the problem with access to the specified file be resolved?