Encoder mode with input capture ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-11-26 1:36 PM
I want to measure speed of motor precisely with encoder pulses and for that I saw this topic
@Werner D�hn @akosodry
and from what I understand here , encoder mode internally triggering another input capture timer
My questions is ;
my encoder has 360 line but multiplex by 4 because of two channel ,so it becomes 1440 puls for one revolution.
I get 1440 puls from timer 4->CNT register but captured2 value from tim5 callback function give 360 puls is it correct ? or is it missing someting ?
and also my rpm measurement range 10-100 RPM so I'm deal with very low frequencies and I'm okay with any suggestions for precise speed measurement in that frequencie range.
Thanks in advance for any solution
/* USER CODE BEGIN 0 */
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1)
{
PPMValue_Prev = PPMValue;
PPMValue = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);
PPM = (PPMValue >= PPMValue_Prev) ? (PPMValue - PPMValue_Prev) : (UINT16_MAX - PPMValue_Prev + PPMValue);
captured2++;
}
}
MX_GPIO_Init();
MX_TIM4_Init();
MX_TIM5_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
HAL_TIM_Encoder_Start(&htim4,TIM_CHANNEL_ALL);
HAL_TIM_IC_Start_IT(&htim5, TIM_CHANNEL_1);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
int i = 0;
int a=0;
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
i = TIM4->CNT;
a=TIM5->CCR1;
HAL_UART_Transmit(&huart2, (uint8_t*)txData, sprintf(txData, "%d\t%d\t%d\t%d\t%d\r\n", a,i,PPM,captured,captured2), 500);
}
/* USER CODE END 3 */
/* TIM4 init function */
static void MX_TIM4_Init(void)
{
TIM_Encoder_InitTypeDef sConfig;
TIM_MasterConfigTypeDef sMasterConfig;
htim4.Instance = TIM4;
htim4.Init.Prescaler = 0;
htim4.Init.CounterMode = TIM_COUNTERMODE_UP;
htim4.Init.Period = 1-1;
htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
sConfig.EncoderMode = TIM_ENCODERMODE_TI12;
sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;
sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;
sConfig.IC1Prescaler = TIM_ICPSC_DIV1;
sConfig.IC1Filter = 5;
sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;
sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;
sConfig.IC2Prescaler = TIM_ICPSC_DIV1;
sConfig.IC2Filter = 5;
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
}
/* TIM5 init function */
static void MX_TIM5_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_SlaveConfigTypeDef sSlaveConfig;
TIM_MasterConfigTypeDef sMasterConfig;
TIM_IC_InitTypeDef sConfigIC;
htim5.Instance = TIM5;
htim5.Init.Prescaler = 84-1;
htim5.Init.CounterMode = TIM_COUNTERMODE_UP;
htim5.Init.Period = 0xffff-1;
htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_DISABLE;
sSlaveConfig.InputTrigger = TIM_TS_ITR2;
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
sConfigIC.ICSelection = TIM_ICSELECTION_TRC;
sConfigIC.ICPrescaler = TIM_ICPSC_DIV1;
sConfigIC.ICFilter = 0;
- Labels:
-
STM32CubeMX
-
TIM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-11-26 11:21 PM
> I get 1440 puls from timer 4->CNT register but captured2 value from tim5 callback function give 360 puls is it correct
I don't use Cube and am not going to decipher your code, but if you set encoder to increment on both edges of both signals (TIMx_SMCR.SMS=0b011), it "sees" four time more edges when the encoder is turned in one direction all the time, than the slave timer's counter, which counts only on one signal's rising edge.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-11-27 1:50 AM
thank for your reply , my problem is both channels activated and both channels rising edge in TIM4 so in this scenario TIM4 counter is successfully measure 1440 puls (it means 100% resolution of encoder) but same time TIM5 captured callback just triggered 360 puls (I manually turn motor wheel one revolution)
but after read your reply , I set tim4 both channels and both edge and tim4 counter "TIM4->CNT value which doesn't seem to count up or down consistently."
the same issiue happened in here (https://community.st.com/s/question/0D50X00009XkdsT/tim4-in-encoder-mode-nucleo-f767zi)
but tim5 callback counter increased 720 puls in one revolution it's like joke !?
(by the way my setup board is stm32f407vgtx)
thanks.