2025-10-27 7:28 AM - edited 2025-10-27 9:13 AM
Hello all
managed to setup the custom display with the STM32H750b-dk, yes the old-original disply was echanged for the new one, connections also via the FC and works well... managed also to create a simple program in Keil and so far so good, the STMs like UTIL_LCD functions are used... anyway would like to move on to the TouchGFX, indeed, have to use to the CUBE IDE, etc. however, wondering how to get around the "Bringing up the custom LCD".
For example, can just the examples for the STM32H750B-DK board be used with a modification of the LCD? In essence only the bigger LCD is used, the driver is actually the same, including the touch... On this note, wondering, if there are templates done that could be used and make configuration for the custom display?
Any comments are more than welcome!
Best.