cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 6.10~6.12.1 can not generate stm32mp157 M4 qspi code

nhappy
Associate II

Cubeide 1.13 and CubeMX 6.9 can generate the valid code for stm32mp157,but Cubeide 1.14 and CubeMX 6.10 can not! is there a bug or the CubeMX 6.10 have some change for stm32mp157?. MCU Package 1.6.0 and the STMH7xx doesn`t affect it. 

void MX_QUADSPI_Init(void) 

{

/* USER CODE BEGIN QUADSPI_Init 0 */

/* USER CODE END QUADSPI_Init 0 */

/* USER CODE BEGIN QUADSPI_Init 1 */

/* USER CODE END QUADSPI_Init 1 */

/* USER CODE BEGIN QUADSPI_Init 2 */

/* USER CODE END QUADSPI_Init 2 */

}

 why?

 

0 REPLIES 0