cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX 4.7.1 + STM32F429xx: FMC/SDRAM RowNumberBits

Michael Steinecke
Associate II
Posted on May 21, 2015 at 10:59

In the CubeMX software, its impossible to configure 13 Bits for address lines (Row bit number). Although the define is existing in the FW library.

#fmc #stm32f4 #cubemx #sdram
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee
Posted on May 22, 2015 at 12:07

Hi Michael,

To be able to configure 13-bit row for used SDRAM, you have to set the ''Address'' for selected SDRAM (Ex: SDRAM 1) to it max value (13 bits) in the Pinout tab.

Then, in Configuration tab (FMC configuration),  you can select ''13 bits'' as ''Row bit number''.

Hope it is clear now.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Michael Steinecke
Associate II
Posted on June 29, 2015 at 11:27

Hi

that helped.

Thanks :)